CIMPLICITY REST API Web Service
CIMPLICITY REST API Web Service / All Operations Resource Group / /projects/{projectId}/objects:read (Post)
Post/projects/{projectId}/objects:read
Description
Gets an array of class Objects that satisfy the filter criteria specified in the request body.
Parameters
NameDescriptionData Type
the id of the projectstring
Request (application/json)

The request body is of type object.

Overview

Filters : ObjectFilter
skip : integer
number of records to skip for pagination
limit : integer
maximum number of records to return
ObjectID : string
provides a wild card string to filter objects by their objectId.
ClassID : string
Class ID for the object provides a wild card string to filter the object list by classId.
Description : string
provides a wild card string to filter objects by their description.
200 Response

The response body is of type ServerSettings.

results from the call

Overview

ServerSettings
The results of the Settings Get.
MaxReadRequestObjects : number
The maximum number of objects that can be read in one call.
MaxWriteRequestObjects : number
The maximum number of objects that can be written in one call.
Fault Responses
FaultDescription
This fault returns a response body of type ProblemDetails.
General error
See Also